This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: is it possible to modify Max Error by the customer without cycling?

Part Number: BQ4050

dears,

some customers reflect that the Max Error could not be programmed by themselves, cycling is a must to update it, thus increasing the cost and affecting the efficiency of the production. they wonder if any method to program the parameters with the learned data and then program the Max Error to 2% and not necessary to cycle every battery pack.

thanks!