This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: SoC deviation

Part Number: BQ34Z100-G1

Hi,

I am using a BQ34z100-g1 with an 8s2p LiFePO4 batteries. The nominal capacity of the battery is 3200mAh.

I have obtained the golden image of the battery and load it in the bq24z100-g1. I have tested the bq34z100-g1 performance during two weeks in a laboratory functional prototype and I have seen twice an irregular performance.

I did a constant current discharge from 100% SoC(and FC bit set) to 10% SoC. The discharge current was 4.4A.

After reaching 10% I stopped the discharge and the systems went in the standby state (30mA consumption). After a few minutes the SoC was 17%.

- Why did this change occur? I supposed It was due to a capacity simulation.

- What parameters are taking into account in this capacity simulation?

Best regards,