Other Parts Discussed in Thread: BQ34Z100
Hi,
I am using a BQ34z100-g1 with an 8s2p LiFePO4 batteries. The nominal capacity of the battery is 3200mAh.
I have obtained the golden image of the battery and load it in the bq24z100-g1.
I sent my system to a controlled temperature test(1000 hours at a temperature of 85ºC). This test is carried out with the system off. When my device returned I checked it and everything was in perfect state but the Bq34z100-G1, that was damage. It did not respone to any communications and we had to replace it.
- What are the possible causes of this damage?
Bes regards,