Hi Team,
Lmzm23601 didn’t seem to start up when pulling greater than 200mA by electoric load(CC mode) in my customer's evaluation using EVM. Could you answer following my customer's questions?
1. Does this device behave as constant current source at start up timing?
2. How much actual load can LMZM23601 drive at start up timing? Is it possible to drive 1A at the timing also?
Here are the their evaluation condition.
Vin : 24V
Vout : 3.3
Load: Electronic load (CC mode)
Issue). Device does not start up with electronic load greater than 200 mA