This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CV Mode Not Working



Hi,

In our application, both AC and USB charger circuits are present and both are supplied with 5.0V through USB. The BCIAUTO is pulled down with 499K. The ADCIN1 pin is left floating. Seperate 4.3V LDO is used with Power selection MUX, one input connected to LDO output and other input conencted to VBAT. The power pins will be supplied the LDO power if USB is present; otherwise it will be supplied with VBAT.

If the battery is not connected USB power is applied, the VBAT pin starts from 0 to 1.2V and stabilizes at 2.0V. As per the CV mode, the voltage should be 4.0V in CV mode. The TPS also not stating UP in this condition.

Can you please clarify what could be the issue.