In reviewing posts regarding the LM5050-1, I came across one that received a response from Aramis Alvarez on 16 June, 2017. In that he states that a TVS diode should be added at the output with the anode of the diode connected to IC ground and not system ground. However in the LM5050-1 data sheet on page 20, figure 31, shows the anode of the TVS diode D2 connected to system ground. There seems to be a discrepancy. Please provide input and/or clarification. Thank you.