1- Can 2 or more LMZ36002 be run in parallel (either to increase load or fault tolerance)?
2- If 2 devices are run in parallel, should the parts be sync'd with clock at 180 degrees? or each part should run independently?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1- Can 2 or more LMZ36002 be run in parallel (either to increase load or fault tolerance)?
2- If 2 devices are run in parallel, should the parts be sync'd with clock at 180 degrees? or each part should run independently?
Thanks
Hi Matthew,
What is your desired application condition (VIN and VOUT)? The LMZ36002 cannot be ran in parallel because it doesn't have an ISHARE pin.
Depending on your package preference there are two options:
For information on how to run these modules in parallel please take a look at the following TI Collaterals:
Regards,
Jimmy