Other Parts Discussed in Thread: TLV755, TPS7A90
Hi team
1. Customer would like to use 100uF cap as output capacitor, because this cap will help when 1-msec instantaneous power failure happens.
Do you recommend to use 100uF cap? If no, what is the reason?
2. Are there any effective ways to deal with 1-msec instantaneous power failure?
3. Are there any recommended devices that can use 100uF cap as output capacitor?
Here is the requirement.
input voltage: 5V
output voltage: 3.3V
output regulation: within +/-2%
Regards,
Noriyuki Takahashi