Hello
I'm using LM25118 in my project. As per my customer's requirement for a 9-30V input, 30V output at 2A is required. Please refer below table.
Parameters | VIN | Vout | Iout |
IC supports | 3-42V | 1.23-38V | <10A |
Considered in design | 9-30V | 30V | 2A |
When I simulated this in TI WEB BENCH simulator I'm not able to get the design. If I take Vin max as 27V or 30.5V I can get the design.
I wanted to know why I am not able to get the design.
Also my customer needs simulation results to be given.
Please help me out in this concern.
Regards
Nidhi P Shetty