This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118: Formulae in datasheet

Part Number: LM25118

Hello



I'm using LM25118 in my project. I'm providing 9-30V input and output is 30.5V at 2A. Iripplemax= 0.9A f=294.6599KHz

In datasheet for all the calculation both buck and buck boost mode calculation is given. With my requirement of current design I need to use buck boost configuration. Is it enough if I calculate all parameters using buck boost?

Why the buck mode equations given?

I thought that it is for the case when input of this IC more than output. Whether what ever I assumed is right.

I have done calculation for both.

When I calculated I1 limit for buck boost it satisfies condition but for buck it is not. I have to undergo iterative method if both calculation required for buck boost?

I wanted to know that if i am using buck boost mode whether buck boost calculation is enough.

Please help me out in this concern.

Regards

Nidhi P Shetty