Other Parts Discussed in Thread: LMG1205
Hello,
I am designing a buck converter (non-isolated) with following specification:
Vin = 24V
Vout = 5V
fsw = 10 MHz
The inductor is going to be planar inductor (spiral with increasing track width). I was asked to choose a half-bridge with an integrated gate driver (preferably GaN devices) and LMG5200 80-V, 10-A GaN Half-Bridge Power Stage is all I could find using TIs designing tools. The reason I cannot use this is because it is impossible to solder in our lab (we lack the necessary technology). Is there a different package available?
Or half-bridges in different technology other than GaN that meets my demands?
Regards,
Girish