This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2000: Supply range

Part Number: BQ2000

Hallo TI,

I wanted to use BQ2000 Battery charger for charging 3 Ni-MH cells in series. In datasheet says, input supply range is between 4 ot 6V and in EVM datasheet says it requires Min 10 V (+DC).

What is specific and right range? Will it work with 5 V input supply?

Please give some feedback regarding that.

  • Hi Mayur,

    The datasheet VCC pin range of 4V to 6V is correct. The EVM has an additional discrete linear regulator circuit to step down the voltage at VCC to below 6V.
  • Hi Jeff,

    Thanks for reply.

    Would it be possible to supply directly VCC pin by 5 V as an input? If yes, what could be possbile output on pin VBAT? I need at least 3.8 V on VBAT.

    Will this IC work with this application?

    Please feeback.

  • Hi Mayur,

    Yes, a direct supply of 5V to Vcc pin should work.

    Yes, if 3.8V is at BAT+, then the IC should be able to work. Make sure the voltage at BAT pin meets the following condition: VLBAT<VBAT<VMCV. A resistor voltage-divider between the battery pack's positive terminal and Vss scales the voltage at BAT pin. Figure 3. in the datasheet demonstrates the resistor-voltage divider network.The EVM can be configured different ways to be used with a variety of battery packs. Section 2 in the user guide describes the jumper connections on the EVM along with resulting operations.