This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27201: 120-V Boot, 3-A Peak, High Frequency, High-Side and Low-Side Driver

Part Number: UCC27201


Hello Sir/Madam,

Greetings!

the application note explained in this above mentioned data sheet consists of voltage divider circuits between the gate of the mosfet and the output of the gate driver IC. and also there are some capacitor of 22pF(may be Coupling capacitor) used 

it would be help full to me if i can know the reason for connecting voltage diver circuit and 22pF capacitors in that circuit.

Thanks and Regards

Divya