This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5430: Radiation emission data of TPS54340BQDDARQ1 and TPS561201DDCR

Part Number: TPS5430
Other Parts Discussed in Thread: TPS54340, TPS561201

HI we are using below two dc to dc converter in our product, we have fail in radiation testing. can you check attached failure data and see if this can be from these above two regulator.

we have used UL/CE certified SMPS modue to convert AC to DC(15V) , and this DC feed to these two regulator to make 4.5V and 3.3V.

we also have on board third radio module which is also FCC certified.

SCH and Layout can share on request on email.RE problem.docx

Thanks