This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

wide range output dc/dc converter

Dear All,

i am working on a dc/dc converter with the bellow charachteristics:

- input voltage= 400 VDC

- output voltage= adjustable from 0 to 400 VDC

- output current= 1 A

- isolated

how can i do such a full range adjustable converter?

Best Regards,

Ras