Other Parts Discussed in Thread: , LM5067
hello
My Customer Request the Reference Design for -48V, 1.6KW.
Load Condition : -48V, 7A
Used TPS23521EVM-001.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Rakesh
I Tested the TPS23521EVM-001 for below Condition.
VIN : -48V
VOUT : -48V
LOAD Current : 7A
When Q2 Gate Enable, It does not operate due to inrush current.
but When the load current is reduced to 2A, it does operate.
TPS23521EVM-001 support the 1.2kw.
What should I do to operate for have 7A load current?
Regards.
You comment that "TPS23521EVM-001 supports start up load less than 1.5A. ... To start higher loads, use PG signal to enable the downstream load."
And according to its datasheet (page 24), "It is critical to keep the downstream DC/DC off while the hot swap is charging the bulk capacitor."
So, I think TPS23521 only allows the sequential ON for downstream load (for example DC-DC module). That is the downstream load should be turned on after hot swap turning on (maybe until charing the output bulk capacitor)
If not, let me know that how the hot swap circuit to turn-on simultaneously with its downstream load (in case that the load is greater than 1.5A)
Dear
I agree with your comment, that is "It is not possible to power up the down stream load while charging large bulk capacitor".
The downstream load would be turned on after some delay. However there seems to have some difference between other hot swap controller and TPS23521.
Assuming that the downstream have bulky capacitance and no sequential turning-on circuit, TPS23521 cannot fully turned on and will enter into hiccup mode. In some other hot swap controller, they will start successfully and after some delay the downstream load will turn-on automatically. The latter needs for no forced delay circuit.
Is it right or wrong?
Thank for your reply.
But you seem to misunderstand my query. I understand that the hot swap and its downstream cannot turn on simultaneously under bulky output capacitance.
Unlike TPS23521, LM5067 never enter into hiccup mode during start-on (although its output capacitance is over 1mF) . Of course LM5067 also have some delay time until its downstream load turns on.
I want to ask another question - that is TPS23521 can handle load of 1600W@48V maximum?
If not, pls recommend proper hot swap IC.