Hi ALL:
Q1:
I want to know if the BQ34110 can distinguish the different capacity batteries with the same chemical. for example, I have some NICAD batteries on my hand,but the batteries have different cell nums and so have different capacity.when the system power on if the bq34110 can go on a Self-learning . by the Self-learning, the BQ34110 can get the battery cell nums and to distinguish the different battery.finnaly I need to write differnt parameters to bq34110 dataflash
Q2:
I want to know if the BQ34110 can distinguish the batteries with the different chemical. for example, I have some NICAD batteries and LiFePO4 batteries hand.when the system power on if the bq34110 can go on a Self-learning . by the Self-learning , the BQ34110 can distinguish the NICAD batteries and the LiFePO4 batteries. finnaly I need to write different parameters to bq34110 dataflash.
I want to use the unified software to manager the different Specification battery!