Please see attached gg and log. Chem ID is 457.
RemCap, FullChgCap, TrueRC, TrueFCC all drop in value during charge when the current is still well above the taper setting (600mA).
At sample 1492, TrueFCC drops from 10120 to 9552 and hold for the duration of the charge
At sample 1493, TrueRC drops from 10105 to 9538, and starts to rise again
At sample 1504, RemCap and FullChgCap both drop from 10119 to 9952 and hold for the duration of the charge.
Any ideas on what setting I have wrong?
Thanks,
Larry Norman