Other Parts Discussed in Thread: TPS61199
Dear TI team,
i would like to use the TPS61197 in my design, in order to control the Backlight LEDs of a specific Display. The backlight voltage or simply said the output voltage of the IC must be up to 46,1V and the TPS61197 should be able to provide ,according to the datasheet of the display, (typically) 545 mA. Could this IC be a solution for my design?? The input voltage of my system is 24 Volts. Are there any equations , in order to be able to calculate if the device can deliver this power (in this case approxímately 23Watts)
Regards,
George