This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21040: IN-DPM feature

Part Number: BQ21040

I want to make sure I understand the IN-DPM feature of this product. The charging source for my application can be any USB charger - from a 500 mA port to a higher current source.  Is it OK to set the charging current to the max (800 mA) and let the IN-DPM feature adjust the current for the particular charging source?

Thanks,

Elizabeth