Other Parts Discussed in Thread: UCC28950
We have designied a PSFB converter of 330W with 360V nominal i/p and 13.2V o/p. While testing we are facing many issues.
1. As soon as i start increasing i/p voltage from say 10V , i observe huge inrush in input current and at 250V i am getting desired o/p. But as soon as we go to our designed range, o/p current goes to 14.5V and but my i/p current is so high that it is causing my mosfet's to fail. Since the IC has i/p overcurent protection and o/p overvoltage protection, we were expecting it to actually stop giving pulses.
2. The wires which connect gate driver to mosfets A,B Cand D is getting so heated up that it is melting the wires. Since we are in the stage of prototype we are implimenting gate driver circuit on separate PCB and integrate gate river card to power circuit using wires.
3. The method how we test our converter goes like this. We first give bias voltage to control card and gate driver card and then we gradually give power to the power circuit starting from 0V. Is this method actually correct? We were thinking of designing a flyback converter for gate driver and control card so that it will operate at our power circuit design range.