Q: I'm uncertain whether the daisy-chained com's can operate between parallel modules rather then only serialized modules of cells? That is, multiple 13S strings in parallel, all sitting at ground.
Will this work?
Thanks in advance!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Q: I'm uncertain whether the daisy-chained com's can operate between parallel modules rather then only serialized modules of cells? That is, multiple 13S strings in parallel, all sitting at ground.
Will this work?
Thanks in advance!
Thanks Mr. Vogt;
I reviewed the document but it doesn't include the scenario I'm questioning. My client want's to use the daisy-chained UART communications just as if there were several stacked modules, BUT in their case, the modules are NOT stacked, but sit in parallel (i.e. all at ground level). I don't see why this would not work, but since I'm not familiar with the daisy-chained comm's inner workings, I'm not 100% certain.
Thanks if you can clarify this.