Dear Jasper,
I'm referring to the tread (RE: MC33063A: The transistor stops switching).
The customer has implemented your suggestion with a manal rework on the board (see the picture), but the results were the same.
at around 300mA there is a short between pin1 an pin2.
Could the manual rework the root source ? Can the part be so sensitive on the presence/absence of the capacitnce ?
regards,
Domenico