Part Number: LMZ21701
Other Parts Discussed in Thread: TPS82130
Dear community!
I am working on a design with Zynq 7000 and our team decided to use LMZ21701SILT to provide stable power supply for +3.3V from +12V. PCB design guide requires to place several capacitors near Zynq power pins in total of 215uF. On the other hand, LMZ21701's datasheet says, that output capacitor should be in range of 10-200 uF, but says nothing (as far as i can see) about whole output capacitance. So the quiestion is can i use LMZ21701 if i place 100uF capacitor near its output pin and leave 215uF capacitance near Zynq, or i should use another DC-DC converter which has bigger allowed output capacitance characteristics?
Thank you for your help!