This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65911: VBAT is not clearly defined in Electrical Characteristics tables

Part Number: TPS65911


Hello,

in the datasheet for TPS65911A (SWCS049S), some electrical characteristics (section 5.6: PWRON, PWRHOLD, GPIO0-8, PWRDN)  are referenced to VBAT voltage that is not mentioned/defined in the datasheet before. Based on the table heading under section 5.7 (saying that "...all VCC inputs set to VBAT voltage...) it can be assumed that the VBAT is the main input voltage supplying most of the VCCx inputs. However in such a case the use of VBAT in section 5.6 is incorrect because the signals PWRON, PWRHOLD, GPIO0-8, PWRDN are supplied either by VRTC or VCC7 (as per section 4.1 Pin Attributes)

Can you please clarify definition of VBAT?

Thank you.

Josef Rypar