Part Number: BQ77915
Hello,
I made a PCB with the BQ77915, but the design does not seem to work.
Test setup:
-5 220ohm resistors with 18.5V psu to simulate
-PCB with BQ77915
-8 ohm load
What happens:
-No load: Output is 18.5V for a second, then drops to 16.2V
-With load: Output almost immediately collapses
What could be the problem?
Schematic:
Q1= NVMFD5C466NLT1G
D4= BAT54C
No jumper are connected, so 5S config.