This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Charging tablet with 5V@3A using USB 2.0 cable...

Other Parts Discussed in Thread: TPS2549, TPS2546

Hi,

I am working on a hardware (which acts as host) where it has USB 2.0 ports and connects to tablet over USB 2.0 (tablet acts as device).

I am able to communicate with tablet (using RNDIS) and need to supply the power it as well. Need of the power supply is 3A at 5V which I would not be able to do from my hardware.

I have a separate power source which can give me 5V - 3A and wnated to know if there is any way I can combine with USB (as there is only USB micro getting connected to tablet) using some thing like Y connector. Or do you have any suggestion using any hub which can do this?

With best regards,
P.