Hi,
I need to design power supply but I don't see Webench tool providing a solution.
the requirements is:
Vin = 5V (4.5~5.5V)
Vout = 100~200V
Iout = 100mA
Can anyone recommend a TI solution?
Thanks,
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
Thanks for your recommendation. It doesn't need isolated output. The UCC2805 is interesting. What is the Fault soft-start?
I prefer current mode controller with programmable soft-start. because it get power from USB port, the input power is limited at 5V 1.5A. The soft start is mast have feature. I don't want the system reset due to the inrush current of this power supply.
I found you have a reference design with TPS61087. It works at the current limit mode during start-up with power from USB. this is what I want it.
I also see anther part like LM5180, which is simplify the flyback design with integrated switch and primary side regulated.
what do you think about those parts? which one will be the best fit?
Thanks,
Jeff
Hi Jeff,
TPS61087 is a low voltage rating boost converter. As the output voltage is too high, you could use a boost controller in flyback topology to realize the conversion.. LM5022 is a good choice.
Hi Jeff,
Since you don't have an isolation requirement a good place to start is this reference design. It uses the LM3481 in a boost configuration with a charge-pump stacked on the output to achieve 200V on the output. This article covers the operation in this configuration. This LM3481 has fix internal soft-start. I think this should be enough soft-start time assuming the output capacitance is fairly small.
The other option is use the LM5155 in the same configuration and is shown in this reference design. The LM5155 has external soft-start that can be programed as needed.
Note that this design only requires a simple inductor and not a transformer like a flyback.
Thanks,
Garrett