Other Parts Discussed in Thread: TPS2561
I have an application with one USB Host port and one USB OTG port. The scenario I have is the OTG port is connected to Host (a PC) . When I power down my device the PC is still providing 5V to my OTG port. This PC VBUS 5V shows up on VOUT2 of the TPS2561 on my board, which I fully expected. But I am also seeing approx. 1.1V at VIN and also VOUT1 of the IC. I measured the current of leakage through VOUT1 and it is about 3mA!
What is the leakage path through the TPS2561? Is this expected? Will the IC get damaged in this use case?
Any suggestions for eliminating the leakage through an unpowered TPS2561? Series diode?
Is there another TI dual USB power switch that doesn't have this leakage path when unpowered while voltage is present on VOUT2?
Thank you,
Greg