This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD88599Q5DC: Symbol footprint for ORCAD

Part Number: CSD88599Q5DC


Hi ,

This is LEBA from NIDEC Corp.

I am under support by TAKIGASAKI ISAO.

May I ask you two question related to DMM0022A package of CSD88599Q5DC.

1) I got the CSD88599Q5DC_DMM_22.bxl file from TAKIGASAKI already and used UltraLibrarion to export to Cadence Allegro tool 17.2.

By *.bat file I can make the drawing files and related files; however there is no symbol file.

I tried to make the symbol file by Orcad PCB Editor and get the error.

Create symbol started.

 WARNING(SPMHA1-301): Create symbol DRC errors exist. 
 Duplicate pin number V. 
 WARNING(SPMHA1-298): Create symbol duplicate pin numbers. 

 ERROR(SPMHA1-291): Create symbol has been aborted.

 Can you help me to verify this error?

2) The second question is the pin that actually used in this device are totally 7 pins (GL, NC, PGND, VIN, GH, SH, VSW).

However, from the drawing we see that there are more than 26 pins. I think there will be warning of "extra pins".

How we can define the pin numbers in drawing file to solve this problem?

Best Regards.

Leba