I am in the final stages of finalizing a design using the BQ20Z65-R1 gas gauge and am basing my circuit off that used in the Evaluation Module for this gas gauge. Before I send the product off for fabrication, there a few minor points which I'd really appreciate if anyone could clear up:
1. The single-point connection to the low-current ground system from the sense resistor:
Should the connection be made at the PACK- side or the 1N side of the sense resistor?
The EVM datasheet shows the connection at the PACK- side while in SLUA534 it is made at the 1N side: which is correct?
2. Can the chemical fuse be put in between PACK+ and the MOSFETS instead of between the top (+ terminal) cell of the pack and the MOSFETS? (as it might be too late to alter my design...)
3. Which capacitor (designator) in the EVM schematic is used to decouple the power supply to the BQ20Z65? C20? C21?
Thanks :) Any help or tips would be appreciated!
Nick