Other Parts Discussed in Thread: LM4132
Tool/software: Code Composer Studio
Hello,
I want generate constant current of 6.094 mA using LM334(3 Terminal). My resistor selection is 22.1 ohm(0.1%) and 221 ohm(0.1%) with V+ is +12 V as per datasheet .
Problem is current always increases from 6.094 mA to 7.038..(on and on) and hence my PT-100 temperature sensor output continuously increases.i want 0.1 C accuracy using PT-100 but as the current continuously increases my temperature get never steady. please help me as early as possible.
Thanks in Advance