This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: BQ76930- TIDA-01093

Part Number: BQ76930
Other Parts Discussed in Thread: TIDA-01093

Hi TI guys

I'm using BQ76930*2 in my 20S packs project,I designed it follow the TIDA-01093.

but there are two questions that need your help, thx.

1,what's the function of Q31?

2,what's the function of Q33?

thx

  • Hi Jack,
    I did not design the circuit, however:
    Q31 allows the charge FET gate to drop below GND_B potential. Without it Q30 would be a voltage follower and the charge FETs would turn on again if the battery voltage was much less than the charger voltage.
    Q33 provides a voltage drop to allow variation of the voltage at the Q32 source without triggering the expedite shutdown circuit (Q34, Q37) mentioned in the TIDA-01093 design guide section 2.1.