This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS610981: The current problem

Part Number: TPS610981


The following figure, VMAIN decreases by 0.1v, resulting in a decrease of 0.3ma in I(ma).Is that normal?

  • Hi Hank:
    I'm sorry, that I don't sure what the I(ma) mean. and what's the meanings of A load/ D load/"后加2K".
    Please share information with more details, such as the load conduction. 
    Sincerely thanks~

  • I(mA) is Iout(VMAIN+VSUB),”D LOAD“ is the LOAD attached to VMAIN,“A LOAD” is the LOAD attached to VSUB. "后加2K" is when you start running with no load, and then you add 2K of load,

    So you should compare the number 1 to the number 7, the number 1 to the number 8.

    At first there is no load, then the load is added, and the current will increase by 0.3ma.Is that normal?

     

  • Hi Hank:
    Thanks for your reply.
    According to the datasheet, Vout is remain in the proper range. It's normal from this view.

    But I still confused the test you listed. You could sent private message to me if you have some concern.