Hi,
Spec require output define 11V/5A and 5V/2A by usb source controller define. But it need to stable work before UVP(3.6V/2A). How to design VDD circuit? There are VDD circuit design in datasheet, p12. Is it suitable for VDD circuit design when output is 3.6V/2A? Or other recommend VDD circuit design?
Spec:
Vin=85~264VAC, 47-63Hz
Transformer turns radio: 40:6 <== it can adjust.
Vout=11V/5A amd 5V/2A
Notice: stable work on 3.6V/2A before UVP.