This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5022: Inductor selection for a SEPIC converter

Part Number: LM5022

Hello,

I am trying to design a SEPIC converter with the LM5022 using your WEBDESIGNER design tool. The basic specifications are these:

  • Input voltage range: 15V-25V
  • Output voltage: 24V
  • Maximum output current 3.5A

The schematic proposed by the tool is the following: : https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=89E4A78AE1183FBA

My question is about the inductors. Specifically, it is the CMX1211Z181B-10. I have not made detailed calculations but I think it is oversized both in the value of the inductance and in the maximum current. Due to layout issues I can not use this component and the design tool does not provide me with another option.


In the LM5022 datasheet I could not find an example of calculating the inductors for a SEPIC converter (only for Boost Converter), so I followed your design guide 'AN-1484 Designing A SEPIC Converter'. Next the steps to size the inductors, I obtain the values ​​of:

  • Dmin= 49.6 %
  • Dmax=62%
  • L1 ripple current = 2.75A
  • L1 = L2 = L = 22 uH
  • The peak input inductor current is for L1 = 7.2A, and for L2 = 4.375A

Based on these values, I understand that the CMX1211Z181B-10 is an oversized component, right?

Because I can not mount a first prototype on a breadboard. Is this inductor SRP1265A-330M  a good choice for both L1 and L2?

Thanks and best regards.

  • Hi FranMartin,

    Thanks for reaching out to us with your questions.

    Your calculations for inductance and peak currents look correct and the inductor selection looks good. It should be fine to use these. Please also note that WEBENCH selects components based on what is in the library.

    Thanks,

    Garrett