This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H100-Q1: max current limit value using external resister

Part Number: TPS1H100-Q1

Hi Team,

Could you help share what's the max current limit when using external resister at CL pin ?

I don't find any data in spec, but seems it's 7A ? Is this 7A tested and ensured for all production parts ?

Currently one customer use it, and test using 330ohm resister at CL pin, but find it's just 5.5A max.

And even by shorting it with 0ohm, it's also just 5.5A max output.

Checked with them that the DC source is not limit, but actually 10A max.

Thanks.