This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90120A: LInux PMBus CD90120a Config Update Tool

Part Number: UCD90120A

I've got some questions related to creating a linux application to perform UCD90120a configuration upgrade via SMBus. 

The application itself is mostly written.

First question: how do I generate the SMBus script file to update the UCD90120a's data flash?

I am only interested in updating the configuration, not the device's firmware.

Is the correct script generated by choosing the following options in TI Fusion?:

“Click to configure device”->”File”->”Export”->”Data Flash Write Script”.

(I have been using "“Click to configure device”->”File”->”Export”->”PMBus Configuration Write Script”.)

(Not sure what this does, but it doesn't update the data flash. Seems like I fell down a rabbit hole trying to use it.)

Second question:

We're using a UCD90120a master+slave configuration.

How do I go about updating both devices, e.g. in which order?

I suspect the system may reboot after upgrading each device?

Should I perform all the upgrade steps short of reset on both devices before performing a reset?

What's best/correct way to deal with this situation?