Other Parts Discussed in Thread: TPS63020-Q1, , TPS63020
Hi Team,
Do we have plans to release this device with a Q1 variant? If so when?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Do we have plans to release this device with a Q1 variant? If so when?
Thanks
Hi Brigitte,
I'm already suggesting that part to my customer - But they have the requirement for a part in EP or HR with a lower quiescent current for a second rail either directly from the battery with a buck/boost or from the output of the 020, operating as a buck.
Output current is roughly 1mA. Any recommendations?
3.3V.
The input can either be from a lithium cell (2-4.3V) or the output of the TPS63020. But it needs to be available as Q1, Extended temp (military) or EP.
From what I gathered, using two 020's appears to be the only solution - but happy to hear about other options.
Hello Carlos,
Shall both output voltages be 3.3V? I still do not fully understand the system. If you do not want to share some data on E2E, you can use lbs_request@list.ti.com to send more details to.
Hello Carlos,
 
 Do I understand correctly that the input voltage can go higher than 4.3V when the charger is applied?
 For these low currents, TPS63020 is for sure an overkill and I think that it is more efficient to use an LDO on the output of the TPS63020 instead of 2 TPS63020.