This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC6C5912: Ground pad for footprint?

Part Number: TLC6C5912


Section 11 of the TLC6C5912 datasheet shows a Layout Example with a large GND fill area under the device, but pin 20 is the only GND pin. Normally a large pour under the chip means there is a GND pad on the bottom of the package, but the package diagrams on pages 21-22 do not show a bottom pad.

Is the Junction-to-board Thermal Resistance just through pin 20?

Thanks,

Lee

  • Hi Lee,
    Yes, you are right. Pin 20 is the only GND pin.
    The effective way to control the temperature is to expedite thermal spreading from cooper to ambient air. That is the reason to maximum the cooper coverage.
    And theoretically, the pin and the cooper that connected to the pin will have the same temperature because of the good thermal conductivity of the metal. one pin is enough for this package.

    Regards,
    Shawn.