This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62175: TPS62175 when opening and shorting the FB terminal resistance, there is a question about VOS operation.

Part Number: TPS62175

Dear support member,

My customer used TPS62175.

I have a question.

When opening and shorting the FB terminal resistance with TPS62175, there is a question about VOS operation.

Q1
When the FB terminal resistance is opened and shorted, what is the IC output voltage when the FB function can not be controlled?

Q2
In the data sheet, it is described as 7.4 V(typ) when the FB pin is open, but is the output voltage controlled at 7.4 V?

Q3
In the explanation, only Typ is listed, but how much is the range?


Best regard.
Bob Lee.