We have questions about TPS65320C-Q1.
Question 1.
We have a question about thermal shutdown.
In datasheet p.7, TSD is 175℃.
But in datasheet p.20 " 7.3.3 Thermal shutdown",
The device implements an internal thermal shutdown as protection if the junction temperature exceeds 170°C (typical).
Which is 175℃ or 170℃ correct?
Question 2.
TPS65320C-Q1 has LDO built in.
Does this LDO have short circut protection?
Short circuit protection : Both DCDC converter and LDO? DCDC converter only? LDO only?
Best regards,
Takahiro Nishizawa