Team,
my customer is using the TPS40211 device as LED driver (min. quantity 100ku/y). He got stuck because of missing informations in the datasheet regarding the internal LDO (Pin BP).
Could you please provide me this additional informations:
- Output Voltage of the internal LDO at Vdd=4.5V - 30V at ILDO_Out=5mA, 10mA, 15mA)
- Saturation Voltage of the LDO at VDD=4.5V - 30V at different Temperatures.
This informations are very important for my customer to win the design. I would highly apprechiate if you could me this set of informations.
Thanks and Regards,
Matthias