Part Number: BQ76PL455A-Q1
Other Parts Discussed in Thread: HALCOGEN, BQ76PL455A
Tool/software: Code Composer Studio
Hello.
We are using the BQ76PL455A-Q1 EVM along with Hercules TMS570LS04 LaunchPad for building a 48V BMS solution. We are working with the BQ76PL455A-Q1 Example Code (Rev. A) provided on the software tab of BQ76L455AQ1 product page. We want to enable CAN communication in the LaunchPad so that communication with an external controller can be done. We have successfully tested the CAN communication between two Hercules TMS570LS04 LaunchPads as per the Hercules CAN tutorials. We now want to include this CAN functionality with the BQ76PL455A-Q1 Example Code. How do we include the necessary header and source files? Is the HALCOGEN file for BQ76PL455A-Q1 Example Code available? How do we proceed?
Thank you in advance.
Regards,
Kartik