Other Parts Discussed in Thread: UCD74120,
All,
Please confirm the size resistor that should be used for AVGG. I see it is recommended between 1 and 2 ohms however what wattage value? I found this used on a schematic for the UCD74120: RES, 2.2 ohm, 5%, 0.063W, 0402. Is this correct for UCD74111? Is it the same recommendation? Also the data sheet says use a resistor between 1-2 ohms? What is the tolerance for this value as I found the referenced resistance value above in a schematic for this part on TI.com.
Thanks,
HSG