This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Design Energy

Part Number: BQ34Z100-G1

Can you please explain the meaning of DesignEnegy parameter.  Pack or Cell?

I have a battery pack that consist of 24 LION cells.  6x cells in series and 4x cells in parallel.  

The specifications for a single cell is is 3.6V (nominal) and 3300mAh (rated).

The pack specifications are thus:

Nominal voltage = 21.6V (3.6V * 6)

Rated Capacity = 13.2 Ah (3.3Ah *4)

Rated Energy = 285.12 Wh (21.6V * 13.2 Ah)

I have selected the DesignCapacity to be the rated capacity for the pack (13200mAh).  Is this correct?

I expect the DesignEnegy to be set to 285120 mWh but I am limited to the max value of 32767mAh.  Do you have a solution for this?