Other Parts Discussed in Thread: GPCCHEM
Hi,
I have recently performed relax-charge-relax-discharge cycle with my 450mAh LiCoO2 battery (4.2V max voltage) using BQ27421-G1A EVM and uploaded the log on GPCCHEM.
Report given best chem ID matching with my battery as 3136 with a max deviation of 1.65%. Apart from that report also given below values
| Generic Chem ID | Device/ Voltage/ Chemistry | max DOD error, % |
| 3142 | bq27421-G1D: 4.4V LiCoO2 | 12.71 |
| 354 | bq27411-G1C: 4.35V LiCoO2 | 14.65 |
| 128 | bq27421-G1A: 4.2V LiCoO2 | 15.83 |
| 312 | bq27421-G1B: 4.3V LiCoO2 | 18.91 |
I have some queries based on the report
1. What is the significance of max DOD error% ?
2. What will be the inaccuracy in the SOC reported by the BQ27421-G1A gauge with my 450mAh battery in the filed ?
3. Why max DOD error% is less with G1D & G1C compared to G1A when my battery is supporting max voltage of 4.2V ?
4. What is the importance of Temperature values in the log file to GPCCHEM tool. Will it impact max DOD error% ?
Let me your feedback.
Thanks & Regards
Vidyasagar
Device / Family #1 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, %3142 bq27421-G1D: 4.4V LiCoO2 12.71354 bq27411-G1C: 4.35V LiCoO2 14.65128 bq27421-G1A: 4.2V LiCoO2 15.83312 bq27421-G1B: 4.3V LiCoO2 18.9
1