Other Parts Discussed in Thread: BQ76200, BQ76940, BQ34110, BQ34Z100-G1
I have made a BMS ,which is made up of BQ78350,BQ76940,BQ76200 and 12 Cells.
When the load is on, AOLDL and AOLD will be set.
I have measured the current at the moment of powering the load with oscilloscope.
The current is less than 9A.
In fact, the RSNS (the resistor between SNSN and SNSP) is only 0.001 ohm.
I must change OCD_T[3..0] to b0100 to be sure AOLDL and AOLD will not be set.
However, OCD threshold is 17mV when OCD_T[3..0] is b0000.
Therefore,I think the threshold should be 17A when RSNS is 0.001 ohm.
Anything wrong?