I just made a DC/DC module with LM5085.
The output is designed to be 12V.
In fact, the output is 12.10V when there is no load.
When the load is on , the output will be up to 12.5V.
When the load current is up to 3A, the output will be changed to 13V.
Besides, the output is stable.
Is it normal for LM5085?