This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28911: re-work EVM for a 15V output

Part Number: UCC28911


Hi,

UCC28911 EVM original design is for a 5V output. Could it be slightly re-worked (tune some resistor) to achieve a 15V output?

Thank you!

- Rocky

  • Rocky

    Yes, UCC28911 EVM can be modified to have 15V output. More modifications besides adjusting the resistor divider to the VS pin is needed though, the turns ratio of the transformer is recommended to be changed and all the output components (D5, C6, R11, C7, C8, R12) are recommended to be recalculated to make sure they have proper voltage rating.

    We recommend using the excel calculator to determine what the new component values should be UCC28911 www.ti.com/.../sluc624

    Best Regards,
    Eric